SCHNEIDER ELECTRIC - DREAM ELECTRICALS AND HARDWARE, PUNE

Schneider Electric - Featured  Products

https://download.schneider-electric.com/files?p_Doc_Ref=ODAE223R_TR&p_File_Type=rendition_288_png&default_image=DefaultProductImage.png

ZENcelo Full-Time Weatherproof Single Gang Socket Cover (Transparent) IP55

https://retailpavilion-in.se.com/schneider-electric---dream-electricals-and-hardware-pune-pune-13926/catalog/products/zencelo-full-time-weatherproof-single-gang-socket-cover-(transparent)-ip55/5120663323934720
Reviews ( 2 )

The Full-Flat form factor has redefined many facets in life. Aero plane seats. TVs. Mobile phones. Electric stoves... And now switches. Aesthetically pleasing flat switches are in fact available.

INR

5120663323934720
https://retailpavilion-in.se.com/schneider-electric---dream-electricals-and-hardware-pune-pune-13926/catalog/products/zencelo-full-time-weatherproof-single-gang-socket-cover-(transparent)-ip55/5120663323934720
0

Schneider Electric

13926

https://d1i0xzxi1l5kaw.cloudfront.net/SE-Opale-2Way-Switch80a5068e-1c40-4664-9806-d61f2709bda2.jpg

Opale Switch 2-Way 6A CG

https://retailpavilion-in.se.com/schneider-electric---dream-electricals-and-hardware-pune-pune-13926/catalog/products/opale-switch-2-way-6a-cg/4518055118897152
Reviews ( 1 )

Opale range has been designed by international designers keeping in mind the local market and its needs. The range gives an exceptional Ease & flexibility of use/installation and freedom to the customer.

INR

4518055118897152
https://retailpavilion-in.se.com/schneider-electric---dream-electricals-and-hardware-pune-pune-13926/catalog/products/opale-switch-2-way-6a-cg/4518055118897152
0

Schneider Electric

13926

https://download.schneider-electric.com/files?p_Doc_Ref=E8331L1LED_WD&p_File_Type=rendition_288_png&default_image=DefaultProductImage.png

AvatarON switch, 16AX, 250V, 1 Way, Led, Wood

https://retailpavilion-in.se.com/schneider-electric---dream-electricals-and-hardware-pune-pune-13926/catalog/products/avataron-switch%2C-16ax%2C-250v%2C-1-way%2C-led%2C-wood/4915528639447040
Reviews ( 1 )

AvatarON offers six fashionable, classic appearances, letting your home's details change, just like the changes in your colorful life. Unique, patented technology and exquisite manufacturing ensure comfortable operation, and the easy-mount design allows you to change the faceplates as quickly and easily as you wish.

INR

4915528639447040
https://retailpavilion-in.se.com/schneider-electric---dream-electricals-and-hardware-pune-pune-13926/catalog/products/avataron-switch%2C-16ax%2C-250v%2C-1-way%2C-led%2C-wood/4915528639447040
0

Schneider Electric

13926

https://download.schneider-electric.com/files?p_Doc_Ref=AAKY1085_IOP-def_WD&p_File_Type=rendition_288_png&default_image=DefaultProductImage.png

Opale Bell Press Switch 6A with Indicator

https://retailpavilion-in.se.com/schneider-electric---dream-electricals-and-hardware-pune-pune-13926/catalog/products/opale-bell-press-switch-6a-with-indicator/5755737421643776
Reviews ( 1 )

Opale range has been designed by international designers keeping in mind the local market and its needs. The range gives an exceptional Ease & flexibility of use/installation and freedom to the customer.

INR

5755737421643776
https://retailpavilion-in.se.com/schneider-electric---dream-electricals-and-hardware-pune-pune-13926/catalog/products/opale-bell-press-switch-6a-with-indicator/5755737421643776
0

Schneider Electric

13926

Articles

1727 / 2

Inclusion is a core value at Schneider Electric, and it shows in the way careers are built here. Kelvin’s journey highli...

On: 2025-06-27
Inclusion is a core value at Schneider Electric, and it shows in the way careers are built here. Kelvin’s journey highlights how a supportive environment can open doors to growth, leadership, and impact. From managing supply chain operatio...

Now your home will know when you’re on your way. Thanks to our GPS-Enabled systems, you can now make sure that the curta...

On: 2025-06-27
Now your home will know when you’re on your way. Thanks to our GPS-Enabled systems, you can now make sure that the curtains are drawn, lights are turned on, and AC is set to cool, right when you come home. #BringHomeTheSmart and automate wi...

Frequently Asked Questions(FAQs)

Q1. What is Schneider Retail Pavilion ?

<p>Schneider Retail Pavilion is the brand name under which Schneider Electric is selling its products, through electrical stores and shops near you.</p>

Q2. How to differentiate power consumption & power dissipation ?

<p>The power Consumption in VA is Bus Current * Voltage And the Power dissipation is "lost" or wasted power, represented by the power converted to lower forms such as heat that are no longer useful in that system. In relation to a power supply the dissipated power is the difference between the input and the output power, as the rest is wasted or dissipated. So power dissipation is not fixed for these hardware but what we can say is it will be approx. 10% of Power consumption on full load.</p>

Q3. How to use RCCB-ID in Three Phase Network?

RCCB-ID can be used for Three Phase Network (220/440V AC).

Q4. Where can i find ISO certificates for all Schneider Electric facilities ?

Please click on the link to download the ISO certificates for Schneider Electric facilities: <a href="http://aafr0251.fr.schneider-electric.com/global/ddi/iso/ISOCERT.nsf/WebFilter.xsp"> Click Here </a>

Q5. What is RCCB and Which type of RCCB is suitable for inverter load?

Electricity has become an indispensable part of our lives, but one cannot ignore that it comes with its share of perils to human life and property. With significant risks like electrocution and fire, protecting electrical circuits becomes necessary, and a Residual Current Circuit Breaker (RCCB ) helps to do so.